Importing a Program from a Library
You can import a function or program defined as a library object into a Program Editor within the current problem. The imported copy is not locked, even if the original is locked.
1. | From the Actions menu, click Import. |
2. | Select the Library Name. |
3. | Select the Name of the object. |
4. | If you want the imported object to have a different name, type the name under Import As. |